7/10/2020 4:26 PM | |
Posts: 7 Rating: (0) |
Hello, there is this discussion on the Node-RED forum where Nick O'Leary (the creator of Node-RED) questions if what Siemens is doing with Node-RED (commercial usage without supporting the Open Source Community) is moral or not: https://discourse.nodered.org/t/visual-flow-creator/29712 Is it true that Siemens is largely using Node-RED, on IOT2020/2040 and most recently on Mindsphere, and it is not supporting the OpenJS Foundation and the whole Community? If yes, is there any plan to do it? |
Last edited by: machadotiago at: 07/12/2020 21:13:35 |
|
7/10/2020 4:50 PM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32886 Rating: (4066) |
You are not allowed to ask the forum this question. This forum is a user forum which Siemens makes available to users and only moderates. The purpose of this forum is that users help other users with technical problems if possible. If you would like an official statement from Siemens, please contact Siemens directly, possibly via a Support Request.
|
Last edited by: ixo65 at: 07/14/2020 07:34:45 |
|
This contribution was helpful to1 thankful Users |
7/10/2020 4:55 PM | |
Posts: 7 Rating: (0) |
Oh, sorry, thanks for the recommendation, we will go on the right way as you mentioned. |
7/12/2020 1:16 PM | |
Joined: 3/30/2011 Last visit: 3/29/2024 Posts: 733 Rating: (255) |
Hello, however this seems to me a very interesting discussion, maybe it can be moved in "meet and talk" forum. Best Regards |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
7/12/2020 9:15 PM | |
Posts: 7 Rating: (0) |
is it possible to move a topic? |
7/12/2020 9:25 PM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32886 Rating: (4066) |
Yes, use the button "Suggestion" under your first post. Then you can write a message to the moderator. |
7/13/2020 12:49 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, I can only speak for the IOT2000 series from a support point of view: Yes, we integrate node-red in our example image, which we are providing. As far as we didn't have anything to adapt here, we can't really contribute. The only thing to invest is legacy care since the IOT2020/2040 is using an old x86 processor. I am answering lots of, lots of basic node-red questions in this forum and if I can't answer I forward the guys to the node-red forum or github pages of specific nodes. I also raised an issue on your S7 node github page. Also this issue was initiated in this forum and I forwarded this guy to your page. So "never ever contributing" is not the whole truth Regarding Flow Creator and the discussion going on in node-red forum I have forwarded this to the involved persons. So your post has now reached the right person and there is an internal discussion ongoing. I personally can't do more in regards of that, sorry. In future I will try to contribute a little more, even if I am just the man-in-the-middle between our customer and your community. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to2 thankful Users |
7/13/2020 2:00 PM | |
Posts: 7 Rating: (0) |
This was the answer I was looking for. Thanks @bergmanu! I even edited my post in the Node-RED forum due to this "new" information. |
7/14/2020 7:31 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7959 Rating: (162) |
Hi all, the question from machadotiago is placed in the right conference, because he asked a general question and a part of it was regarding IOT2020/ 2040:
From my point of view the question could only be answered from our Expert bergmanu, what he has already done Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on