7/5/2020 4:06 AM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating: (19) |
Hello, I Hope all is good for you and your famillies. I will like to ask, if in your experience is there any special precaution or consideration i have to take care before changing control mode of my Sinamics G120 from ¨Dynamic Drive control´ (P1300=20) to ´U/F Control with Linear Characteristics (P1300=0)? (I will perform the change when the system is Off). The reason for doing such change is because i have observed that actual speed does not follow speed set point very well, please se attached picture (MDI_Drive_Accel_Curve). In the other hand i have another drive which is set in U/F control mode, this drive seems to have a better performance (Please see attached picture TDI_Drive_Accel_Curve). Can you please give your advices and oppinions on this? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/06/2020 09:41:41New subject after splitting Keep working! |
|
7/5/2020 4:08 AM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating: (19) |
My appologies, i did not attached the MDI_Accel_Curve picture. Here It is. Once Again thanks a lot. |
Keep working! |
|
Follow us on