7/18/2020 9:09 AM | |
Joined: 11/9/2018 Last visit: 6/10/2024 Posts: 6 Rating: (0) |
I,m facing a problem while trying to connect with IOT2040 via PUTTY, the system IP i have configure as same as the default sub-net. but here when i try to ping the default IP of IOT2040 it's unreachable. So now how i can i reset the IOT to its default form. I tried to reset using file "ConBox_Commands.json" which i found in iot2040 manual for reset then also I'm not able to communicate via putty ????!!!!!!! if any one have a solution plz suggest ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/20/2020 06:17:42New subject after splitting |
|
Follow us on