7/21/2020 4:17 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201) |
Is the program stored in EPROM? Then can it be, that the program create the DBs in the runtime. |
7/21/2020 6:41 PM | |
Joined: 11/8/2018 Last visit: 8/8/2024 Posts: 6 Rating: (0) |
How it works? In any function in program doesn't exist instruction assign states of physical addresses to data in db64. |
7/21/2020 6:52 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201) |
See attachment.
AttachmentS5-100U Manual page 192.pdf (306 Downloads) |
This contribution was helpful to1 thankful Users |
7/21/2020 8:01 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201) |
Hello Miki95, is your problem now solved? |
Follow us on