7/22/2020 8:35 AM | |
Joined: 11/14/2018 Last visit: 10/31/2023 Posts: 502 Rating: (68) |
Hello mcandeo, this discussion might help you: Beside that, it's important that you give information about the WinCC you're using. (Basic/Comfort/Advanced/Professional). When you ask a question, you can basically always have a look at the following post, it explains which information are needed: Regards, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
This contribution was helpful to1 thankful Users |
8/13/2020 2:21 PM | |
Joined: 8/3/2009 Last visit: 4/24/2024 Posts: 12839 Rating: (1639)
|
Hello If you have a Comfort/Advanced Project: https://support.industry.siemens.com/cs/de/en/view/57025748 If you have a WinCC Professional RT Project then you can use a Combobox Object and load the Values with a VB Script like this (Script Context is for example in the same Screen in Event Screen Loaded): Dim ComboObj and so on, its just a small example to guide you i the right direction. And next Time a few more Information would be very nice... Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on