7/23/2020 7:31 PM | |
Joined: 6/25/2020 Last visit: 3/25/2023 Posts: 3 Rating: (0) |
Hello, I just bought a Logo8 and started to do some trials, but I have problem with the SD card reader. When I try to download a LWE web page here's the error: When I chek the diagnostics from the logo display, it says: "Card detached" The big problem comes now: I tried to extract the SD card from its slot, but it seems blocked, as if the SD card slightly came out and prevents the slot from opening. What can I do? I do not want to destroy the SD card slot by trying to open it with strength. Thanks for the support. Roberto. PS: the data logging is working. I can upload from Logo data log files (but probably they are not stored in the SD card, aren,t they?)... ------------------------------------------------------------------------------------------ |
Last edited by: Roversette at: 07/23/2020 19:38:20Last edited by: Jen_Moderator at: 07/24/2020 06:25:03New subject after splitting |
|
7/23/2020 9:10 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32844 Rating: (4061)
|
The card slot is a bad construction, that is sure.... |
Follow us on