7/23/2020 6:10 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33005 Rating: (4078)
|
Attached a simple example for set timer over LOGO! display. If you now want to change a parameter, you need to select the appropriate message text. When the message text is selected, press the ESC key for longer than 2s. Then, a black bar appears in an input / output field. With cursor up / down you can choose between several fields. If you select the field to change, press the OK button (at TDE > Enter). The black bar turns now in a blinking box. With cursor up / down, you can now change the value at this position, with cursor left / right to switch the position. When you are finished with the changes, press again the OK button and you will return to the black bar. Now you can select with the cursor up / down to another field, or press ESC to quit the operation.
AttachmentTimer_set_over_display_0BA8.Standard.zip (70 Downloads) |
Last edited by: ixo65 at: 07/23/2020 18:10:39 |
|
This contribution was helpful to1 thankful Users |
7/23/2020 11:07 PM | |
Joined: 2/6/2014 Last visit: 7/4/2022 Posts: 236 Rating: (3) |
Thank you very much, I'll give a try ! |
7/24/2020 5:24 AM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33005 Rating: (4078)
|
I wait for you feedback ... |
7/24/2020 9:21 AM | |
Joined: 2/6/2014 Last visit: 7/4/2022 Posts: 236 Rating: (3) |
It works. thank you ! |
This contribution was helpful to1 thankful Users |
7/24/2020 9:25 AM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33005 Rating: (4078)
|
That sounds good.... |
This contribution was helpful to1 thankful Users |
Follow us on