7/25/2020 11:14 AM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
Hello ChemE; To achieve AS-Wide interconnection, you must "merge" your networks in the multi-project. May be by sharing the below information, will be possible to provide an appropriate suggestion. Are both the CPU assigned under single project or in two different single projects? Which type of controller they are? And, What type of data have you been shared between these controllers and used in their associated charts as I/O's? (like Global DB info, I/O Image table info) Are you trying it in real hardware or with simulation? Please tell us more about the data you have shared and how... The formal step would be: 1. Merger the plant bus network "If its multi-project" 2. Create a connection between "AS" (Mention right detail in the connection, like Rack, Slot number, IP address, Controller name) 3. Download and monitor the connection status from NETPRO in runtime. 4. Apply the logic to perform data exchange according to the chosen network methodology. |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
Follow us on