7/28/2020 12:46 PM | |
Joined: 4/28/2015 Last visit: 12/8/2022 Posts: 10 Rating: (0) |
Good afternoon, forgive help. The situation is as follows: WinCC server is installed at the factory, it interrogates 4 PLCs (2 simatic S7-1200, 2 Schneider Electric m340). 2 clients are connected to it, through a network environment, without a separate project on the client's PC. This system works, but periodically a message appears about the lack of communication with the simatic and / or schneider. I eliminated some of the errors, the rest I don't even understand what it is. The IT department says that all equipment is constantly pinging and no connection loss was found, but in the Scada Log files I find a message about a disconnect and a huge ping. I am sorry to help find and fix the problem. I attach the log files. P.S. Messages like this are not specifically clear: 2020-07-24 00:54:00,269 ERROR - FlexChan RQ OnEndOfRequest RQ not found: RQID=28194 - ModBus
AttachmentSIMATIC_S7-1200__S7-1500_Channel_02.txt (87 Downloads) |
7/28/2020 12:47 PM | |
Joined: 4/28/2015 Last visit: 12/8/2022 Posts: 10 Rating: (0) |
AttachmentWinCC_Sys_03.txt (115 Downloads) |
7/28/2020 12:48 PM | |
Joined: 4/28/2015 Last visit: 12/8/2022 Posts: 10 Rating: (0) |
AttachmentModbus_TCP_Channel_01.txt (134 Downloads) |
7/28/2020 1:41 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello StudAsu, the CCWriteArchiveServer.exe, which writes data from Taglogging and This has nothing to do with the problem of the modbus, This needs a more detailed investigation. You should use the SIMATIC Assessment Suite - Data Collector (SAS-DC) https://support.industry.siemens.com/cs/ww/en/view/65976201 Then create a Servicerequest, and send the data to the
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
8/15/2022 6:10 AM | |
Joined: 4/1/2021 Last visit: 8/18/2022 Posts: 2 Rating: (0) |
Hello. Can you tell me what to do with the error: CCWriteArchiveServer,[(null),224]failed to insert into MSARCLONG with 0x80004005(#0,'2022-05-27 02:45:46.540'), MSG_STATE_COME |
8/15/2022 1:12 PM | |
Joined: 8/3/2017 Last visit: 5/3/2024 Posts: 1085 Rating: (53) |
Hi Kirya, you quoted the answer for your error message What isn't clear for you? |
Last edited by: 8Noodles at: 08/15/2022 13:14:01Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
8/16/2022 7:47 AM | |
Joined: 4/1/2021 Last visit: 8/18/2022 Posts: 2 Rating: (0) |
Hi 8Noodles, there are no solutions to my problem in this post. There is only what it refers to, and the solutions proposed do not fit my problem |
Follow us on