7/27/2020 1:24 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi HBCM_, it depends on the sensor that is connected, not on the output of the sensor. The difference between 2-Wire and 4-wire-transducers is that the 2-wire-transducers have their power supply through the measurement-wires. Thats the reason why only 4..20mA-range can be used with it. 2-Wire-transducers need the measurementrange-module in D 4-Wire-transducers need the measurementrange-module in C You can find this information in following manual: SIMATIC S7-400 Automation System Module Datahope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
7/30/2020 6:16 AM | |
Joined: 10/25/2019 Last visit: 5/20/2024 Posts: 278 Rating: (20) |
nice. |
Follow us on