7/20/2020 2:29 PM | |
Joined: 7/13/2011 Last visit: 2/29/2024 Posts: 11 Rating: (0) |
Try to install the update 12 for Wincc 7.4 SP1. After that you can open the wincc Explorer |
7/21/2020 8:58 AM | |
Joined: 3/20/2019 Last visit: 8/10/2024 Posts: 6 Rating: (0) |
Thanks also facing the same problem server not connect after uninstalling wincc and installed back problem solved |
7/24/2020 3:49 PM | |
Joined: 10/3/2010 Last visit: 9/19/2024 Posts: 1562 Rating: (191) |
Autostart on a multiuser client (v7.4 SP1 update 9 / Windows 10 1809) works perfect. However manually opening the project from the server on the client fails with "server not available" message? |
B r g d s , |
|
7/31/2020 10:21 AM | |
Joined: 10/3/2010 Last visit: 9/19/2024 Posts: 1562 Rating: (191) |
No logical explanation for this kind of behaviour? Manual open server-project on the client does not work on 1 of the redundant servers (server not available message" but with autostart everything works... |
B r g d s , |
|
8/6/2020 5:34 PM | |
Posts: 2 Rating: (0) |
Hello Can I ask what version is your win 10? thanks |
8/12/2020 11:24 AM | |
Joined: 10/3/2010 Last visit: 9/19/2024 Posts: 1562 Rating: (191) |
As said above: WinCC v7.4 SP1 update 9 / Windows 10 build 1809 |
Last edited by: SteBo at: 09/30/2020 09:13:46B r g d s , |
|
9/30/2020 9:21 AM | |
Joined: 10/3/2010 Last visit: 9/19/2024 Posts: 1562 Rating: (191) |
Reminder: Autostart on client works on both redundant servers Interconnect through Simatic Shell on the client works on both redundant servers Manual opening server project from WinCC Explorer on the client without project gives error: "Server not available" Manual opening server project from systray icon gives error: "The project could not be opened. Error: Project is not open" PMStart.log: 2020-09-30 09:02:24.724 PM( 3636-13836) Open project failed (0x80046605) PMStop.log: 2020-09-30 09:02:23.295 PM( 3636-13836) Open project started 2020-09-30 09:02:24.725 PM( 3636-13836) Open project failed (0x80046605) 2020-09-30 09:02:24.726 PM( 3636-13836) Close project called 2020-09-30 09:02:24.726 PM( 3636-13836) Caller: OpenProjectByName2 2020-09-30 09:02:24.898 PM( 3636-13836) ProjectClose - All applications notified. 2020-09-30 09:02:24.982 PM( 3636-13836) Stop applications 2020-09-30 09:02:24.994 PM( 3636-13836) All basic applications are stoped (94 ms)! 2020-09-30 09:02:25.044 PM( 3636-13836) Close project finished (0x0) This behaviour is not on a single client but on several clients. |
B r g d s , |
|
10/15/2020 3:00 PM | |
Joined: 6/3/2018 Last visit: 6/14/2022 Posts: 5 Rating: (0) |
Hi Georg, All files are available. I copied from other PC using project duplicator. |
Follow us on