8/2/2020 12:49 PM | |
Posts: 1 Rating: (0) |
what needs to be done for my analog input unit to automatically connect to the diagnostic unit MODE I insert a check mark when compiling the CFC function "Generate module drivers" and doesn't help. ------------------------------------------------------------------------------------------ |
Last edited by: Gnf at: 08/02/2020 12:49:47Last edited by: Gnf at: 08/02/2020 14:11:49Last edited by: Jen_Moderator at: 08/03/2020 10:03:11New subject after splitting |
|
8/3/2020 10:30 AM | |
Joined: 3/13/2015 Last visit: 4/22/2024 Posts: 122 Rating: (38) |
Dear, You should use PCS 7 approved IO modules (including interface modules). You can find them here: If using PDM it also possible you have selected HART functionality but did not declare a PDM device. Regards, |
This contribution was helpful to1 thankful Users |
Follow us on