8/4/2020 9:01 AM | |
Posts: 7 Rating: (0) |
now I'm using version 4 of Simatic Automation Tool. during the scan of my network I find the equipments which are in the same sub network as the PC on which Tool is launched. on the other hand I would like to find also the equipments which are on another sub network. by making a manual addition of an equipment by its IP address, I have the following problems. 1: no connection could be established with the device. 2: After a scan, Tool displays the device with a different mac address ( 00:08:E3:FF:FC:50) which is confusing because it's the @ mac of a cisco device. NB: 1: my CPU is a 1516 and it's well part of the supported devices catalog. 2: ping operations or access to the web interface are done correctly. Hence the question 1: For adding a device, which port does Tool use? 2: Tool must necessarily be executed on a PC running on the same subnet as the devices ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/04/2020 11:12:53New subject after splitting |
|
8/4/2020 11:13 AM | |
Joined: 6/19/2017 Last visit: 5/3/2024 Posts: 8006 Rating: (163) |
Best regards, Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on