8/4/2020 4:59 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello Elshen; Are you talking about a Lenze drive as part of a Profinet network? Which drive model exactly? Which communication Card (the document below mentions a MC-PND for Profinet)? Did you use Lenze software "Engineer" to commission the Profinet communications on the drive? Did you download and integrate the GSDML file for the drive in your Step 7 hardware cpnfigurator? Have you setup the Profinet (IP) address and Profinet Name of the drive in both configurators with the same data? Have a look at the following document from Lenze, for Profinet communications) and study the basic requirements. https://download.lenze.com/TD/PROFINET__Controller-based%20Automation__v1-6__EN.pdf Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/04/2020 17:01:02 |
|
This contribution was helpful to2 thankful Users |
8/4/2020 6:01 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
and which CPU you use? S7-300, S7-1200, S7-1500, ? |
This contribution was helpful to1 thankful Users |
Follow us on