8/5/2020 8:05 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (375)
|
Hi, I haven't found any particular node for this sensor. But maybe this one can help you. All the other i2c node available are either for particular devices or for the Raspberry Pi. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
8/5/2020 4:33 PM | |
Joined: 8/30/2019 Last visit: 4/8/2022 Posts: 2 Rating: (0) |
Thank you bergmanu. I install from Node Red Manager Pallette node-red-contrib-johnny-five module without any problem. For use with IOT2040 additionally i need to install galileo-io hardware suport. For this i use this command "npm install galileo-io johnny-five" After reboot Node Red didnt start even i try to do this manualy. I think the problem in error when i install galileo-io (screenshot in attachment) Could you help to fix it? Rev1 Small remarks. I find that Node Red stop working after add j5-function and put where some code. I can use j5-gpio-out with i2c read function. Could you help with filling i2c address? |
Last edited by: SRSer at: 08/06/2020 07:39:48 |
|
Follow us on