8/30/2020 10:55 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hi, in this case I would recommend to create a service request and send the SDT data to the technical support: https://support.industry.siemens.com/cs/ww/en/sc/2090 Regards |
Grundkurs/Systemkurs WinCC V7: |
|
3/10/2022 4:36 PM | |
Joined: 3/29/2018 Last visit: 3/7/2024 Posts: 1 Rating: (0) |
I have the same issue with WinCC V7.5 SP2 Upd 7. I contacted siemens support but no luck. has anyone found the issue? |
3/18/2022 2:58 PM | |
Joined: 8/3/2009 Last visit: 5/13/2024 Posts: 12933 Rating: (1646) |
Hello nunobnk I would to clean the project: https://support.industry.siemens.com/cs/de/en/view/109763043 and https://support.industry.siemens.com/cs/de/en/view/109775466 then check also in SQL Server management Studio if there are some wrong inked Databases left after closing the WinCC project. you can also try to copy the project with project duplicator then the RT Files are also deleted. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on