7/31/2020 3:54 PM | |
Joined: 5/22/2019 Last visit: 3/7/2024 Posts: 2 Rating: (0) |
I have purchased these converters, but I can't get it working. I connect it as follows: Encoder Converter PLC A (or B) -------------> NPN terminal "+" terminal---------------> 24V "-" terminal -------------->DI0.6 (or DI0.7) The sensor is also supplied with 0 and 24V Should I connect M1 with 0V too? All help highly appreciated ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/03/2020 06:26:55New subject after splitting |
|
Follow us on