7/22/2020 1:25 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, The attachment shows you have not installed CFC V9.0 SP1 |
If I could help you, you can use the RATE button. Thank you. |
|
7/22/2020 4:54 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Yes, you can easily see that your installed CFC version under "installed software" is V9.0 and not V9.0 SP1. So if your project is with SP1, you need to upgrade the software version. In your case it means you need to have PCS7 V9.0 SP1. A separate install of CFC is not available. |
If I could help you, you can use the RATE button. Thank you. |
|
8/8/2020 1:25 AM | |
Joined: 7/15/2017 Last visit: 2/14/2024 Posts: 13 Rating: (0) |
Thanks very much |
Follow us on