5/31/2014 2:26 PM | |
Joined: 9/27/2006 Last visit: 5/4/2024 Posts: 12257 Rating: (2666)
|
Hello aasim` Have a look at the contents of this recent discussion on the forum: Replacing SM321 online in S70-400H system Hope this helps, Daniel Chartier |
5/31/2014 4:17 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
Hellomostref, CIR feature is different. Thy guy here don't want to use this feature. He would like to change the module in Run mode "Hot Swapping" fature. CiR is Configuration in Run which is completly different.
I afraid this info is not correct. Simply if you hit "F1" for all these OBs, you will know that you do not need all these OBs for allawing insert / remove feature. For example, OB40 to OB47 are HW Interrupt OBs. What is the relation between HW Interrupt OBs and Hot Swapping? OB 81 is for Power Supply error. And if you did not inserted, it won' affect the hot swapping feature.
|
Last edited by: Ayman Elotaify at: 5/31/2014 4:22 PMLast edited by: Ayman Elotaify at: 5/31/2014 4:18 PMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
Follow us on