8/9/2020 6:26 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (267) |
Dear Ad_181......., May be you never change the unit? Can you take a look at the cfc chart of the respective blocks ? look for something call PV_Unit, you did not change the default figure "1001" to other units right? Press F1 at that place and search for the unit code. The advantage of having "Unit" in integer is , when you want to change the unit during development stage or commissioning stage, for example from bar to mbar at the later stage when you realize mbar is a better representation, you do not need to configure the "Text" and do OS Compilation / download anymore. In APL, you can straight away change the value in "PV_Unit" in online test mode, then the value will automatically changed. This is a great improvement as compared to old version of PCS 7. I provided you a table below, you may take a look and configure your unit properly. hope this is helpful for you. AttachmentPV_Unit.pdf (170 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on