2/13/2020 8:11 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello; You are using RS 232 connections and want to connect to 2 slaves? This will not work, RS 232 is limited to a single slave node. "RS-232, when compared to later interfaces such as RS-422, RS-485 and Ethernet, has lower transmission speed, short maximum cable length, large voltage swing, large standard connectors, no multipoint capability and limited multidrop capability." https://en.m.wikipedia.org/wiki/RS-232 Hope this helps, |
This contribution was helpful to1 thankful Users |
2/13/2020 8:18 PM | |
Posts: 3 Rating: (0) |
1500 is the master and Eaton is slave. Nothing else. MRu |
8/11/2020 11:27 AM | |
Joined: 2/11/2019 Last visit: 9/9/2022 Posts: 1 Rating: (0) |
Did you come right? |
Follow us on