7/27/2020 5:59 PM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
If you use a S7-1500 (S7-1200 should work too): see attachment, all three files include the same information in different forms. Attachment2 word to INT.zip (388 Downloads) |
Last edited by: miami at: 07/27/2020 19:20:28 |
|
This contribution was helpful to1 thankful Users |
8/12/2020 7:54 PM | |
Joined: 8/14/2019 Last visit: 2/18/2024 Posts: 6 Rating: (2) |
So sorry for the late reply, work's been mad and I don't seem to have received an email notification of the thread being replied to. A BIG thank you for the SCL however I made a slight mistake in my original post; I am taking the data in as UINT not WORD. I've attached a screen grab of the collected data (The relevant registers are Slave 6[2] and [3] being 30003 and 30004 respectively) with 790L shown on the gauge. **** HOLD ON. ***** After another quick stab at this I now have it working following the key part/ issue which was combining the 2 Words (or as stated above, UINT) together following your annotated SCL. After a couple of minor adjustments I can confirm it is WORKING.... Attached is a picture of the Input data I'm reading over Modbus, the SCL and finally the function block. THANK YOU FOR YOUR HELP!!!!! AttachmentFuel_Conv.pdf (423 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on