8/12/2020 5:50 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Absolutely. Which PLC/CPU are you using and how are the drives commanded to JOG? |
8/12/2020 6:06 AM | |
Joined: 5/27/2020 Last visit: 8/17/2023 Posts: 5 Rating: (0) |
I use S7-1516T CPU. Drive is using S210. I use the speed axis for drive and MC_MOVEJOG for JOG function. |
8/12/2020 12:30 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Thanks for the clarification. This is above my pay grade and it's best answered by others. |
8/13/2020 1:36 AM | |
Joined: 5/27/2020 Last visit: 8/17/2023 Posts: 5 Rating: (0) |
Do you have an example file for that? |
8/13/2020 10:50 AM | |
Joined: 4/28/2015 Last visit: 10/20/2023 Posts: 43 Rating: (6) |
Usage of Pre-PostServo is described in this example: Using the MC-PreServo and MC-PostServo organization blocks It also shows how to connect a datablock to a technology object. |
Grüße, Axel |
|
Follow us on