8/15/2020 8:57 AM | |
Joined: 9/3/2008 Last visit: 4/25/2024 Posts: 920 Rating: (157) |
Hi Nikola, Just an additional thing since you mentioned that downloads did occationally not work. Do you or anyone else ever access any of the servers with Remote Desktop (RDP)? If so, this might be the problem for the download issue. Make sure RDP cannot be used. If remote access needs to be used for the servers, then use for example VNC: How do you access WinCC and PCS 7 plants with "RealVNC"? |
Michael |
|
Follow us on