11/28/2019 1:34 PM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
do you have another machine? try to do the same action and check to see the problem able to be repeated again? |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
11/29/2019 3:49 AM | |
Posts: 57 Rating: (0) |
Dear JazTai, I don't have another machine with PCS-7 Installed. I have to sort out problem on this Machine only. |
11/29/2019 5:16 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
maybe you could check in you C:\Programfile\siemens\wincc\diagnose. check any error in the logs file and try to understand them one by one. You can also attach here some more information. Normally for window issue, you would need to check the software compatible with the window or not. Which pcs 7 versions and window are you using? Compatibility Tool Probably you could also try reinstalling the software. It will be good to install in a fresh new window with built-in administrator rights. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/16/2020 12:56 PM | |
Joined: 3/4/2015 Last visit: 12/27/2023 Posts: 3 Rating: (0) |
Hell Everybody I am also have the same problem. Please Help!!! |
8/17/2020 2:46 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
And then? what have you done to troubleshoot the problem? |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on