8/21/2020 11:04 PM | |
Posts: 1 Rating: (0) |
Can the S120_CU320_2_PN have 3 DRIVES connected, with a 352 telegram each one?... because when I write from the PLC I can only write to the first one and the other 2 cannot write to them?... is there any example with a PLC Control logix and S120_CU320_2_PN with 3 drives in the same bus. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/24/2020 08:47:33New subject after splitting |
|
8/24/2020 7:46 PM | |
Joined: 7/7/2010 Last visit: 9/18/2024 Posts: 15204 Rating: (2417) |
I routinely have multiple S120/G120 drives connected via PN using telegram 352. Each one has its own unique hardware ID, and each telegram has its own unique datablock. Like Drive1_Telegram352_DB, Drive2_Telegram352_DB, Drive3_Telegram352_DB
|
science guy |
|
Follow us on