8/26/2020 9:05 AM | |
Posts: 6 Rating: (0) |
Dear sir, a very good afternoon. I have a MM440 DRIVE 5.5KW connected with PLC S7 200 .Terminal 29 and 30 of this drive are connected with other two mm440 in parallel and this goes to PLC. USS connection.Now I want to replace one drive with G120,pm240-2.My doubt is ,which is the corresponding terminal of G120 where I should connect these two wires which are connected to 29 and 30 of mm440. Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/26/2020 14:05:14New subject after splitting |
|
8/26/2020 2:08 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Best regards, Jen_Moderator |
Follow us on