8/26/2020 10:38 AM | |
Posts: 39 Rating: (0) |
Yes.
AttachmentDIA.zip (321 Downloads) |
8/26/2020 11:13 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, I see there was an error with the PLC connection which could be caused by: The logical device is not defined in the registry. An error was displayed on the OS which can be the following reasons: - The connection has been aborted by the channel, because a VMD status of the CPU (STOP, HALT, or DEFECT) has been recognized. Is the CPU OK? There is also an error with the taglogging: failed to insert into MSARCLONG with 0x80004005 I see that you have three network cards installed. How are you operating the plant: Separate plant and terminal bus? Only the Plant bus should be configured in NetPro, the terminal bus settings are entered in Simatic Shell. Maybe some settings are wrong on the ethernet cards... There is also an error with the script functionality of the server. Are there any custom scripts used? Try to disable them and try WinCC runtime without those scripts. There is a problem with the PCS7CustomPicture directory. A few EMF files are faulty or cannot be called:
I think the station configuration is not loaded properly from the ES to the OS server project via PLC->Configure and PLC->Download. PLCnames cannot be found. An unknown error occurs on the server: 6.08.2020 16:35:48.235 OSLTMHandlerX.exe TID[1240] [SAM OSLTMH] OnWinCCProjectActivate() - SEVERE PROBLEMS DURING STARTUP! Shutting down ... 6.08.2020 16:56:27.871 OSLTMHandlerX.exe TID[8720] [SAM OSLTMH] ForwardMessage() - InitIVAR2Interface failed. Reason: <Unspecified error> Can your OS server handle the RAM memory? Could be an issue of not enough free RAM memory. Are all users and passwords the same for ES and OS? After typing all this text above, I notice the following error: 2020-08-26 10:16:22.355 PM( 2792-07492) OS Version: Windows 8 Unknown Edition (build 9200) - 64-bit Are you running a compatible OS version?? Which one are you running for the ES and OS? If the OS version is correct (but the error says it's not), I suggest you create a SR and follow the steps in the following link using the Simatic Assessment Suite Data Collector Tool. https://support.industry.siemens.com/cs/ww/en/view/65976201 |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
8/27/2020 7:05 PM | |
Joined: 2/29/2016 Last visit: 3/12/2024 Posts: 100 Rating: (1) |
Wow, How did you diagnose that?? |
Follow us on