8/31/2020 5:01 AM | |
Joined: 3/13/2019 Last visit: 9/22/2024 Posts: 158 Rating: (2) |
Dear Expert, In one of my project In FB25(having instance DB25) there are four multiple instance FB205(having instance DB 205) called. I tried to monitor one of FB instance (#STAT23) by using debug menu call up path...but i am little bit confused to select the path and which DB no to be select to open db in menu. As in attached file there is four instance of FB 205(STAT23,STAT63,STAT103,STAT146) in single FB25 thats why i am confusing......pls suggest me how i can monitor individual instances. Regards Pankaj Tiwari Attachmentezyzip.zip (98 Downloads) |
9/3/2020 5:30 AM | |
Joined: 10/7/2005 Last visit: 9/24/2024 Posts: 3022 Rating: (1054)
|
Hi Pankaj Tiwari try the following:
|
Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on