9/2/2020 1:23 PM | |
Joined: 7/9/2020 Last visit: 11/12/2022 Posts: 2 Rating: (0) |
Hi Folks, I am attempting to use the Modbus TCP library on a S300 to cyclically talk to 3 different Modbus TCP devices - with very little luck. I've been able to talk to one device at a time (1 or 3), but not all three cyclically. My understanding is I need to call upon the modbuspn block and with updated parameters each query, but I can't quite get it right. To make matters worse I have limited Siemens experience - I think I'm close but missing something minor (misunderstanding of the unit parameter? correct block interrogation?). If someone could take a peak at my code and advise where I'm going wrong I would be forever great-full. Code is in Step7 5.5 SP2 AttachmentBooster.zip (362 Downloads) |
Last edited by: AllanPeever at: 09/03/2020 10:15:18Last edited by: AllanPeever at: 09/03/2020 10:16:45 |
|
9/3/2020 1:25 PM | |
Joined: 7/9/2020 Last visit: 11/12/2022 Posts: 2 Rating: (0) |
Thank you Wüstenräuber! With your guidance I was able to get it working correctly. |
Follow us on