9/5/2020 9:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, You should have post this query in SINUMERIK CNC automation systems product conference as you mentioned your NCU type is 840D SL. In 840D SL, sinamics drive data is stored in NCU & not in HMI. User need to clear drive data & reload the same. If you want to reload series start up data, in such case, user need to check what back up data user is having? i.e. If series data has all data back up data i.e. NC, PLC, HMI, drive as combine data then user can not reload only drive data. So check what type of series data you have. Above & all, do you have any safety integrated features in installed drive? Please check. By the way, why you want to reload only drive data? What problem do you face? Please be sure before deleting/reloading data. HTH |
This contribution was helpful to1 thankful Users |
9/8/2020 8:37 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please provide NCU& CF card MLFB number along with system software details. |
Follow us on