11/27/2020 2:56 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hallo muneeb, the display in the block editor depends on the editing language set in the project languages. If your project has multiple project languages and you want to open your project on another PC with a different user interface language of STEP 7 (TIA Portal), the system automatically switches the editing language in the project languages too. Check also the properties of the CPU. In the properties by “Multilingual support” you can choise the project language. After choise (example german) compile the device configuration and make the download again. See also the FAQ: In STEP 7 (TIA Portal), why are the display texts, titles and comments no longer displayed after opening the project in the block editor? With best regards |
Follow us on