9/14/2020 9:23 AM | |
Posts: 4 Rating: (0) |
Hi, I have similar problem right now. I give the command. The star and main contactor turn on. After some time delta contactor does not get on and it stops and star-main contactor get off and gives feedback error. But this is not happening all time. Sometime I give command and it works fine.Sometimes it does not work and I cut off electricity and try a few times and it works. The feedback signal is giving from delta contactor. Motor is 200kW. I thouht simocode is not working well so I replaced with a new one. Old simocode version is V2.0 while new one is V3.2. I do not kow this can cause this problem but when I replaced simocode with new one, I still had the same problem. I found another simocode with version V2.0 and it is working fine now. So I do not know the main problem. If the problem is version, how can I work with new version. I will appreciate if you guys can help me. Simocode: 3UF7010-1AU00-0 ------------------------------------------------------------------------------------------ |
Last edited by: mbaranicin at: 09/14/2020 09:27:44Last edited by: The Helping Hand at: 09/15/2020 13:14:32New subject after splitting |
|
Follow us on