9/8/2020 1:48 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
HelloS@G@R, for the ES no WinCC-Station will be createt, without you For the stand alone OS you need to configure a "WinCC Appl.". For a redundant pair of Servers you need to configure a "WinCC Appl." For the Clients you need to configure a "WinCC Appl. Client"
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
9/14/2020 1:01 PM | |
Joined: 4/6/2016 Last visit: 9/11/2024 Posts: 83 Rating: (15) |
Hello Georg, This is first time i am using AS-OS configuration. In my case ES is used for configuration. Also i want to use it as OS client. Isit possible? if yes how can i configure it? |
Many Thanks, |
|
Follow us on