9/16/2020 10:39 AM | |
Posts: 2 Rating: (0) |
I have PROFIBUS FAULT on ET200S 151 standard, which many times is stopped with following indications: LED BF 2 times pulses of 0,5s then 1 pulse of 1s then 5 times of 0,5s then SF 3 times pulses of 1s. can you help us to identify where is the problem. ------------------------------------------------------------------------------------------ |
Last edited by: sozo20 at: 09/16/2020 10:40:34Last edited by: The Helping Hand at: 09/16/2020 12:55:35New subject after splitting |
|
9/16/2020 11:18 AM | |
Joined: 10/7/2005 Last visit: 5/12/2024 Posts: 3005 Rating: (1048)
|
Hi sozo20 how to decode the LED error display for an IM151-1 is explained in THIS manual. |
Cheers |
|
This contribution was helpful to1 thankful Users |
9/17/2020 12:40 PM | |
Posts: 2 Rating: (0) |
Thank you, i think it's very helpful |
Follow us on