9/17/2020 5:27 AM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33809 Rating: (4200)
|
Hello MGumiero, at first welcome to the forum. FS is the German abbreviation for production status (FS = Fertigungsstand). Normally begins a new series of LOGO! with the production status FS01. Until the LOGO! 0BA8 of the first generation was still the same. The 0BA8 of the first generation (LOGO!8.0, Release 09.2014) is a 0BA8 standard as hardware in the LSC device selection. They are available with production statuses FS01-FS03, the firmware versions are V1.08.01 to V1.08.03. A firmware update was not possible. The LSC version was V8.0. Then, in October 2016, the second generation 0BA8, called LOGO!8.1, appeared. It still had the same order numbers as the 0BA8 of the first generation, but the hardware in the LSC device selection is a LOGO!8.FS4. The LSC version was V8.1. The production statuses were FS04 to FS06. Here was the break with the numbering of the production status. According to the previous regulation it should have been FS01-FS03. The numbering of the firmware versions was as by the old system. The versions are V1.81.01 (FS04) to V1.81.03 (FS06). A firmware update has been possible since LOGO!8.1. The current LOGO!8.2 was published in October 2017. The order numbers have now been changed. In the case of the first and second generation LOGO!s, the order number ended with 0BA8. In the case of LOGO!8.2, the order numbers end with 08-0BA0. The old system was reintroduced for the production statuses, and they started again with FS01. The firmware versions are V1.82.01 (FS01) and V1.82.02 (FS02). The LSC version was V8.2 for FS01 and is now V8.2.1 for FS02. To complete the chaos with the firmware versions, there are now also security firmware updates for LOGO!8.1 and LOGO!8.2. The new, upcoming LOGO!8.3 should first be presented at a trade fair in autumn 2019. Then the performance date was postponed to April 2020 (Hannover Messe). However, since the Hannover Messe was canceled due to COVID-19, this was also omitted. LOGO!8.3 should now appear in October 2020 (I hope). AttachmentVersions of 0BA8.txt (475 Downloads) |
Last edited by: ixo65 at: 09/17/2020 05:31:27 |
|
This contribution was helpful to3 thankful Users |
12/12/2021 8:14 PM | |
Joined: 10/22/2021 Last visit: 11/3/2023 Posts: 4 Rating: (0) |
So for us stuck with the 0BA8.Standard a.k.a. LOGO!8.0 FS01 (fw v1.08.01) we can do nothing to protect the devices from the following vulnerabilities:
Source: https://www.helpnetsecurity.com/2019/05/31/siemens-logo-vulnerabilities/ |
12/12/2021 8:17 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33809 Rating: (4200)
|
And what are new details for your post? |
12/12/2021 8:30 PM | |
Joined: 10/22/2021 Last visit: 11/3/2023 Posts: 4 Rating: (0) |
Notifying for the CVEs |
12/12/2021 8:35 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33809 Rating: (4200)
|
But what this to do with the topic? "Firmware version logic (FS:0x)"! |
Follow us on