9/4/2020 11:00 PM | |
Joined: 9/4/2020 Last visit: 6/11/2022 Posts: 6 Rating: (0) |
Hi, I installed image v2.6.1 and I am trying to use the Intel GPIO nodes. I tested with the Intel user button and user LED nodes and it works correctly but I when I try the digital inputs DI0-DI4 only DI4 works. All DI have the same settings. Is there a problem with the Intel GPIO nodes or there is something I am not doing correctly? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/07/2020 09:28:59New subject after splitting |
|
9/9/2020 3:18 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, I remember we had some problems with reading I/Os when using the Inten_gpio nodes in the past, but writing should work. Kind regards! Attachmentnode-red-contrib-IoT2000-gpiov2.zip (453 Downloads) |
9/17/2020 8:45 PM | |
Joined: 9/4/2020 Last visit: 6/11/2022 Posts: 6 Rating: (0) |
What nodes are you guys using on IOT2040 Siemens i/o module? Are these nodes installed on the latest image (V2.6.1)? |
9/22/2020 9:07 PM | |
Joined: 9/4/2020 Last visit: 6/11/2022 Posts: 6 Rating: (0) |
Sill have only only DI4 working. Maybe I will try with V2.6 image |
Follow us on