9/20/2020 9:26 AM | |
Posts: 1 Rating: (0) |
Hi I am currently struggling with a G120C PN drive on Starter, I want to set up a simple jog function with a push button, now I'm setting up everything in the wizard either as a 2wire forw/rev of fixed speed setpoint 2, then I push jog and the motor ID starts generating, but once that is finished when I press the button the drive spools up but no power is going out to the motor. If someone can help with a diagram if setting it up I would appreciate it. Jan ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/22/2020 09:02:47New subject after splitting |
|
9/23/2020 4:07 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello Jan, please check out chapter 6.9 of the G120 operating instruction manual. https://support.industry.siemens.com/cs/ww/en/view/109757226 Basically this shows you the necessary parameters to realize jogging on the G120C. |
With best regards, |
|
Follow us on