9/20/2020 2:33 PM | |
Joined: 12/6/2006 Last visit: 7/8/2024 Posts: 92 Rating: (0) |
All CPU is rebooting due to Data Inconsistency The reboot is happening once in a week and couldn't ablt to find some solutions Attahced the Diagnosed Buffer Details Request your Help AttachmentDiagnose.txt (130 Downloads) |
9/20/2020 3:14 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, The error is coming from FB915. Is this a Siemens block or custom made? In case it's a Siemens block, please check out the following thread: It is possibly related to a license issue. If it is a custom made block, the block should be diagnosed. |
If I could help you, you can use the RATE button. Thank you. |
|
9/20/2020 5:18 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello Iyyapan S; W#16#A090 is an error code linked to the Modbus PN driver, indicationg a missing license key. This error code appears very often in your diagnostic buffer. How do you establish a Modbus/TCP communication from a SIMATIC S7-300/S7-400 and where can you find further information? https://support.industry.siemens.com/cs/ww/en/view/22660304 "Missing or incorrect licensing If you enter an incorrect registration key or no activation code at all, the SF-LED (for S7-300 and IM151-8) or INTF-LED (for S7-400) of the CPU flashes and a cyclic entry is made in the diagnostics buffer regarding the missing license. The error number for a missing license is W#16#A090." Please pay special attention to andress' last posts in the link provided by Oreca. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/20/2020 17:26:57 |
|
Follow us on