9/23/2020 8:15 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, You should have post this query in SINUMERIK CNC automation systems product conference. BTW, have you enetered all machine data, mechanics data of axes correctly? Have you carried out drive tunning, motor ideentification correctly? Since NC, PLC data is very important, you need to entered all data correctly, carry out drive tunning, identification then only machine can run smoothly. If in house expertise is not available, I suggest you to get help from OEM & reload NC, PLC data. HTH |
This contribution was helpful to1 thankful Users |
9/25/2020 6:05 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello, Since your controller is 828D SL, this controller is Sinumerik CNC product catageory as such all queries related with it are posted under SINUMERIK CNC automation systems. A axis Sinamics drive & motor data which you mentioned is identified by Sinamics CU system during identification. Apart from this, user need to configure NC data like axis machine data e.g. number of encoders installed, connected, type of encoder i.e. rotary or linear, is encoder direct or thru gear trench, specific active encoder for axis position feedback, axis mechanics, e.g. ballscrew itch, applicable gear stage, is axis rotary or linear, max accleration, velocity, rapid/feed rate, overide, referencing, etc. etc. Based on this data, NC controller controllers axis motion. So please check, if A axis related axis machine data entries so that A axis will be operational smoothly. Please refer SINUMERIK 828D SINAMICS S120 machine data manual which shall help you to understand setting of NC machine data. HTH. |
Follow us on