9/23/2020 9:42 AM | |
Joined: 11/5/2018 Last visit: 9/5/2024 Posts: 4 Rating: (0) |
Hello all, I'm reliving the old topic because same subject. Trying to use a UDP Broadcast communication between a S7-1200 and another brand PLC which support UDP communication, I have some error while using the TCON module. I always get the 16#80A4 error meaning the IP address distant is not valid. When I check the variable I can see the IP isn't found by the code even if the project is configured. What device need to be chosen to configure the network interface on the network & devices window please ? Enclosed the config. Here the project. https://we.tl/t-3pfvvkQgWU Thank you for the help ! BR ------------------------------------------------------------------------------------------ |
Last edited by: Antoine001 at: 09/23/2020 09:47:16Last edited by: Antoine001 at: 09/23/2020 09:53:11Last edited by: Jen_Moderator at: 09/29/2020 12:17:10New subject after splitting |
|
9/29/2020 12:19 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject UDP broadcast communication is published within the conference Communication / Networks. Best regards,Jen_Moderator |
Follow us on