9/25/2020 4:05 PM | |
Joined: 9/19/2014 Last visit: 11/13/2023 Posts: 70 Rating: (0) |
Hallo, can I ask also help in the program? I need make R F 31.2 a little bite later. I can't understand practice way (without timer). I understand the program count and compare cycle but how i can do it. In which point? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/28/2020 11:20:43New subject after splitting |
|
9/25/2020 4:30 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201) |
See attachment ... |
This contribution was helpful to1 thankful Users |
9/25/2020 6:18 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201) |
And the format of this two DWs is KF. |
This contribution was helpful to1 thankful Users |
9/25/2020 6:46 PM | |
Joined: 9/19/2014 Last visit: 11/13/2023 Posts: 70 Rating: (0) |
Thanks a lot! |
This contribution was helpful to1 thankful Users |
Follow us on