9/27/2020 3:00 PM | |
Posts: 3 Rating: (0) |
Hi Im using plc with siwarex module. I did the device conf and there is no error. Now I want to read its inputs and outputs and the weight. How Can I do that without siwarex tool software or etc.? PLC : S7-1200 DC/DC/DC 6ES7 212-1AE40-0XB0 v4.1 Siwarex WP231 7MH4960-2AA01 Note : I know the function block example but when I copied that to my project. There is an error about firmware version about plc. I think the example version is 4.1 and my plc is v4.4. Help pls. Thanks, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/28/2020 13:26:59New subject after splitting |
|
9/28/2020 1:29 PM | |
Joined: 6/19/2017 Last visit: 4/24/2024 Posts: 7967 Rating: (162) |
Closed cause question posted twice. The second thread with the subject SİWAREX WP231 WITH TIAPORTAL V13 is published within the conference Process Instrumentation / Analytics / Weighing Systems SIWAREX. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on