9/28/2020 2:29 PM | |
Joined: 5/3/2017 Last visit: 2/2/2024 Posts: 673 Rating: (216) |
Hi Atul Gupta, the APL has no block, which shows the information about the CPU status in WinCC. These information is only available with the Maintenance Station (see the Manual PCS 7 Maintenance Station at the chapter "AS/System" area). But you don't have to worry for the Maintenance Station Basic you don't have to buy additional license (For the different version of the Maintenacnce Station see the Manual PCS 7 Maintenance Station at the chapter Application, version and configuration). With regards |
This contribution was helpful to3 thankful Users |
Follow us on