9/28/2020 2:50 PM | |
Joined: 7/9/2019 Last visit: 2/13/2023 Posts: 10 Rating: (0) |
I am not sure what you mean. I definitely have it set up as an encoderless servo. Are you saying this will not work? |
9/28/2020 3:50 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Hello, in Servo mode the ramp function generator is not activated by default. But you can implement it by activating the extended setpoint channel, see chapter 4 of the S120 function manual. https://support.industry.siemens.com/cs/ww/en/view/109771805 |
With best regards, |
|
9/28/2020 7:47 PM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14629 Rating: (2348) |
There is probably a secret to it, but I have always had to start over with the configuration wizard in Starter to get the extended setpoint channel activated. In the point where you are selecting options to add to the drive model, adding the extended setpoint channel is available, and once checked and configuration completed, the RFG is available.
|
science guy |
|
Follow us on