9/29/2020 8:55 AM | |
Joined: 10/3/2010 Last visit: 9/18/2024 Posts: 1561 Rating: (191) |
Check task manager on a regular base to see if WinCC processes are eating memory or CPU. If you are using c-scripts, you might have a problem with destroying memory, causing script.exe to crash. check if script.exe is running whenever WinCC is freezed |
B r g d s , |
|
9/29/2020 8:59 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello Avadh, this can have different possible reasons. If you need help for analyzing the data, you should use the SIMATIC Assessment Suite - https://support.industry.siemens.com/cs/ww/en/view/65976201 Then create a Servicerequest, and send the data to the
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on