9/30/2020 7:13 AM | |
Joined: 8/21/2014 Last visit: 6/10/2024 Posts: 139 Rating: (1) |
Hi, In our project we want to use a third party motor with sinamics S120 drive. The motor is from harmonic drive(FHA-11C). Our siemens sales person suggested us a single motor module of 3A (6SL3120-1TE13-0AD0). Enocoder is of TTL type. We want to make sure that the motor is compatible with the selected sinamics motor module. Also, what needs to be used to connect encoder to motor module(SMC20?) Motor, encoder technical details are in the attachment. Also manufacturer recommended settings for sinamics parameter are also included. But voltage is not mentioned!. AttachmentHarmonic Actuator technical Info.pdf (245 Downloads) |
9/30/2020 10:23 AM | |
Joined: 3/9/2012 Last visit: 9/24/2024 Posts: 96 Rating: (8) |
In SERVO- mode you can parametrize the SINAMICS without voltage (p304). |
Follow us on