10/1/2020 12:32 PM | |
Joined: 11/29/2018 Last visit: 8/7/2024 Posts: 10 Rating: (1) |
Hi Jay I think this manual will be a good starting point. SIMATIC S7-1500 Software Controller CPU - Document ID number: A5E32565315-AG Depending on the configured version of IPC, you should have a soft PLC on it, e.g. CPU 1507S. You can then program this PLC in TIA portal to control the I/Os (ET200SP modules) on the Profinet/Profibus network. Regarding the sensors, there are many different manufacturers. You need to start with an answer to what do you want to achieve with this proximity sensor, what is the environment it will operate in, then you can start looking for a suitable sensor and lastly you need to select a suitable ET200SP card for it. |
Last edited by: DavidDK at: 10/01/2020 12:39:49added a bit about the sensors Last edited by: DavidDK at: 10/01/2020 12:55:46added a pic from TIA16 Please Thank & Rate if you find my post helpful. |
|
This contribution was helpful to1 thankful Users |
Follow us on