10/4/2020 7:50 AM | |
Joined: 5/8/2017 Last visit: 4/23/2024 Posts: 14 Rating: (0) |
Hi everyone In my one substation project, I am using Siemens IEC61850 block in my project. In WinCC, some parameters and Alarms are coming from this block, and some Parameters and alarms coming from my PCS7 alarm block. In the Wincc alarm window both alarms are coming(PCS7 and IEC61850) but in both alarms, the timezone is different by -5:30. I have also attached a screenshot of the alarms window. Can anybody suggest to me, How to show the same time on Wincc no time difference. I also attached the PDF of the Installed Software. Best Regards, ------------------------------------------------------------------------------------------ Attachmentattachement.zip (57 Downloads) |
Last edited by: Jen_Moderator at: 10/05/2020 10:43:35New subject after splitting |
|
10/5/2020 10:55 AM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8018 Rating: (163) |
Closed cause question posted twice. The second thread with the subject Alarm time zone difference +5:30 in wincc from IEC61850 and PCS8.2 Alarm Block. is published within the conference Process Control Systems SIMATIC PCS 7. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on