10/3/2020 3:51 PM | |
Joined: 9/11/2020 Last visit: 1/25/2024 Posts: 24 Rating: (0) |
Best, I want to be able to change te on and off times via the web editor interface. how do i set this up? |
10/3/2020 4:44 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (4197)
|
The hex number is a trouble. The format hh:mm is not possible in one I/O filed. You must make two I/O fields, byte by byte. In attachment an example. To remove the "#" see this topic: AttachmentWeekly timer on LWE.zip (705 Downloads) |
10/3/2020 5:57 PM | |
Joined: 9/11/2020 Last visit: 1/25/2024 Posts: 24 Rating: (0) |
i only see then two times the hours in stead of hours and minutes |
2/5/2022 9:23 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (4197)
|
Which LWE version use you? |
Follow us on